Keysight 89600 VSA .NET API
ChangeInputDomains Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Input Class : ChangeInputDomains Method


Glossary Item Box

Changes the Measurement to be loaded using a subset of the requested input domains.

Overload List

OverloadDescription
ChangeInputDomains(InputDomains)Changes the Measurement to be loaded using a subset of the requested input domains.  
ChangeInputDomains()Changes the Measurement to be loaded using a subset of the allowed input domains.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also