Keysight 89600 VSA .NET API
ChangeLogicalChannelsByCount Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Input Class : ChangeLogicalChannelsByCount Method


Glossary Item Box

Changes the input channel configuration for the current measurement by specifying the number of logical input channels.

Overload List

OverloadDescription
ChangeLogicalChannelsByCount(Int32)Changes the input channel configuration for the current measurement by specifying the number of logical input channels.  
ChangeLogicalChannelsByCount(Int32,Int32)Change the input channel configuration for the current measurement by specifying the number of logical input channels and the sequence count (if using them as sequential input channels). The total number of logical channels will be the logical input channel count times the sequence count.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also