| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property PreferredInputDomains As InputDomains | |
| C# | |
|---|---|
public virtual InputDomains PreferredInputDomains {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property InputDomains PreferredInputDomains { InputDomains get(); void set ( InputDomains value); } | |
InputDomains flags not supported by Measurement.SelectedAnalyzer in current channel configuration will be ignored. Note, this does not cause the current Measurement to be loaded again. Such action may be triggered by ChangeInputDomains(InputDomains) or by actions like recalling a setup file or changing input channel configuration. The currently active input domains are indicated by ActiveInputDomains. Note: Specifying a value of InputDomains.None indicates no input domain preference, and all supported input domains are considered. If input domain capabilities are added to future MeasurementExtension or Measurement.SelectedAnalyzer implementations, they will be included. If this is undesirable, and specific input domain selection is important to maintain behavior backwards-compatibility, it is recommended to specify a value other than InputDomains.None.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.00