Keysight 89600 VSA .NET API
CloseTo(Double,Double) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MarkerCollection Class > CloseTo Method : CloseTo(Double,Double) Method


x
X pixel location.
y
Y pixel location.

Glossary Item Box

Return the closest visible marker to the passed pixel location.

Syntax

Visual Basic (Declaration) 
Public Overloads Overridable Function CloseTo( _
   ByVal x As Double, _
   ByVal y As Double _
) As Marker
C# 
public virtual Marker CloseTo( 
   double x,
   double y
)
C++/CLI 
public:
virtual Marker^ CloseTo( 
   double x,
   double y
) 

Parameters

x
X pixel location.
y
Y pixel location.

Return Value

The closest marker, or null if no markers are visible.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.60

See Also