| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsConsolidate As Boolean | |
| C# | |
|---|---|
public abstract bool IsConsolidate {get; set;} | |
Data values in a 3G Code Domain Power measurement result that are not at the base symbol rate are contained in multiple points in the trace. If the trace is shown in bit reverse code order, then these points will be next to each other. If the code order is Hadamard, then these points will be spread out through the trace. If IsConsolidate is True, then a marker will be shown at all points for this data value (same code channel / symbol rate).
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)