Keysight 89600 VSA .NET API
SelectedItem Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MarkerCollection Class : SelectedItem Property


Glossary Item Box

Gets or sets the selected Marker.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property SelectedItem As Marker
C# 
public abstract Marker SelectedItem {get; set;}
C++/CLI 
public:
abstract property Marker^ SelectedItem {
   Marker^ get();
   void set (    Marker^ value);
}

Remarks

The selected marker has the keyboard focus. Returns null if no marker is selected.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also