Returns a list (pairs of x- and y-values) of all the peaks.
Syntax
Parameters
- peakOrder
- Order of returned peaks, either by ascending X-values or by descending Y-values.
- maximumPeakCount
- Maximum # of peaks to return (no limit if maximumPeakCount <= 0).
Return Value
Returns an array of x- and y-values, one for each peak. If no peaks are found, then an empty array is returned
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 18.50
See Also