Keysight 89600 VSA .NET API
WaitForMeasurementsDone() Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementCollection Class > WaitForMeasurementsDone Method : WaitForMeasurementsDone() Method


Glossary Item Box

Wait 10 seconds for all of the measurements to complete.

Syntax

Visual Basic (Declaration) 
Public Overloads Overridable Sub WaitForMeasurementsDone() 
C# 
public virtual void WaitForMeasurementsDone()
C++/CLI 
public:
virtual void WaitForMeasurementsDone(); 

Exceptions

ExceptionDescription
System.TimeoutExceptionA TimeoutException will be thrown if all of the measurements are not complete within the specified number of milliseconds.

Remarks

For non-averaged measurements, one cycle is all that is required. For averaged measurements, the average must complete.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 15.0

See Also