| Overload | Description |
|---|---|
| WaitForMeasurementsDone(IEnumerable<Measurement>,Int32) | Wait for all of the specified measurements to complete. |
| WaitForMeasurementsDone(IEnumerable<Measurement>) | Wait 10 seconds for all of the specified measurements to complete. |
| WaitForMeasurementsDone(Int32) | Wait for all of the measurements to complete. |
| WaitForMeasurementsDone() | Wait 10 seconds for all of the measurements to complete. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)