Keysight 89600 VSA .NET API
Data Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > MeasurementData Class : Data Property


Glossary Item Box

Gets or sets the Y data points

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Data As Array
C# 
public abstract Array Data {get; set;}
C++/CLI 
public:
abstract property Array^ Data {
   Array^ get();
   void set (    Array^ value);
}

Remarks

Returns the data in its native format. FloatData and DoubleData returns the data in the specified format.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also