Keysight 89600 VSA .NET API
InputDomain Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : InputDomain Property


Glossary Item Box

Gets a value indicating what kind of input data the analysis part of the measurement requires.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property InputDomain As InputDataDomain
C# 
public virtual InputDataDomain InputDomain {get;}
C++/CLI 
public:
virtual property InputDataDomain InputDomain {
   InputDataDomain get();
}

Remarks

For Spectrum input domain data use Measurement.Spectrum.Frequency instead of Measurement.Frequency to setup frequency related parameters.

This property indicates the input domain that the analysis part of the measurement requires and is using. But, the data acquisition part of the measurement may be capable of using other input domains and converting within the measurement before the analysis part to the input domain required for the analysis part of the measurement. See the ActiveInputDomains to get an indication of what the current input domain is for the data going into the pre-analysis part of the measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.50

See Also