Keysight 89600 VSA .NET API
IsCalculateMeasurementData(String) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class > IsCalculateMeasurementData Method : IsCalculateMeasurementData(String) Method


dataName
Name of the measurement data.

Glossary Item Box

Gets a value indicating whether the specified measurement data is calculated even if not displayed.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function IsCalculateMeasurementData( _
   ByVal dataName As String _
) As Boolean
C# 
public abstract bool IsCalculateMeasurementData( 
   string dataName
)
C++/CLI 
public:
abstract bool IsCalculateMeasurementData( 
   String^ dataName
) 

Parameters

dataName
Name of the measurement data.

Return Value

Whether the measurement data is calculated.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also