Keysight 89600 VSA .NET API
IsCalculateMeasurementData Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : IsCalculateMeasurementData Method


Glossary Item Box

Set whether the passed measurement data is calculated even if not displayed.

Overload List

OverloadDescription
IsCalculateMeasurementData(String,Boolean)Set whether the passed measurement data is calculated even if not displayed.  
IsCalculateMeasurementData(String)Gets a value indicating whether the specified measurement data is calculated even if not displayed.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also