Returns the measurement data for the passed data name.
Syntax
Parameters
- dataName
- The data name.
Return Value
Returns the measurement data if the data name is valid, otherwise null.
Remarks
Example
| C# | Copy Code |
|---|
using (MeasurementData data = app.Measurements.SelectedItem.MeasurementData("Syms/Errs1"))
{
if (data != null)
{
string[] summaryNames = data.SummaryNames;
for (int i = 0; i < summaryNames.Length; i++)
{
object summaryData = data.Summary(i);
if (summaryData != null)
{
// do something with the data...
}
}
}
} |
| VB.NET | Copy Code |
|---|
Dim data As MeasurementData
data = app.Measurements.SelectedItem.MeasurementData("Syms/Errs1")
If (Not (IsNothing(data))) Then
Try
Dim summaryNames As String() = data.SummaryNames
For i As Integer = 0 To summaryNames.Length - 1
Dim summaryData = data.Summary(i)
If (Not (IsNothing(summaryData))) Then
' do something with the data
End If
Next
Finally
DirectCast(data, IDisposable).Dispose()
End Try
End If |
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also