Keysight 89600 VSA .NET API
Record() Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class > Record Method : Record() Method


Glossary Item Box

Pauses the current measurement and start recording the input data.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Sub Record() 
C# 
public abstract void Record()
C++/CLI 
public:
abstract void Record(); 

Exceptions

ExceptionDescription
System.InvalidOperationExceptionMeasurement cannot run concurrently with selected measurement (Measurement.IsConcurrent = false).

Remarks

This measurement must be able to run concurrently with the selected measurement (app.Measurements.SelectedItem) or a System.InvalidOperationException will be thrown.

To stop recordings in progress, use Measurement.Pause() or MeasurementCollection.Pause().

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also