Keysight 89600 VSA .NET API
Record Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Measurement Class : Record Method


Glossary Item Box

Pauses the current measurement and start recording the input data.

Overload List

OverloadDescription
Record()Pauses the current measurement and start recording the input data.  
Record(String)Pauses the current measurement and start recording the input data to a specified file in sdf format. The file extension is auto generated. Usually, the extension has the format of 'sdf.integer.integer' Measurement.Record()  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also