| Visual Basic (Declaration) | |
|---|---|
Public Overloads MustOverride Sub RecallFile( _ ByVal fileName As String, _ ByVal format As String _ ) | |
Parameters
- fileName
- Specifies the file name.
- format
- Specifies the file format.
The current recording, in SDF format, is overwritten. SetCenterSpan is called as part of this method.
Supported File Formats:
| format | Description |
|---|---|
| "CSV" | CSV (Comma delimited) [*.csv] |
| "E3238S" | E3238S Time Snapshot [*.cap] |
| "MAT" | MAT-File [*.mat] |
| "MAT7" | MAT-File (HDF5) [*.mat, *.hdf, *.h5] |
| "BINF" | BINF (Little Endian Real32 Binary) [*.binf] |
| "N5110A" | N5110A Waveform [*.bin] |
| "N5106A" | N5106A Waveform [*.bin] |
| "SDF" | SDF (Fast) [*.sdf, *.dat] |
| "TEXT" | Text (Tab delimited) [*.txt] |
| "VITA49" | VITA 49 [*.vita49] |
Note:
MAT may be used instead of MAT7 for recall trace/recording (the matlab file format is auto detected for recall).
If the format is an empty string, then the application automatically determines the file format by looking at the file suffix.
If this is not sufficient, then the file is scanned to determine the format.
If the format cannot be determined or you specified an unknown format, then an error is raised.
VITA49 is only supported since release 2023 Update 2.0 (version 27.40).
For more information about file types, see the "Supported File Formats" topic in the application help.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)