Keysight 89600 VSA .NET API
RecallFile Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Recording Class : RecallFile Method


Glossary Item Box

Recall the current recording in the specified format from a file.

Overload List

OverloadDescription
RecallFile(String,String)Recall the current recording in the specified format from a file.  
RecallFile(String,String,String)Recall the recording for the specified measurement in the specified format from a file.  
RecallFile(String,String,Boolean)Recall the current recording in the specified format from a file.  
RecallFile(String,String,RecordPaddingType,Single)Recall the current recording in the specified format from a file and pad the recording according to the paddingType.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also