Keysight 89600 VSA .NET API
RecordLengthTime Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Recording Class : RecordLengthTime Property


Glossary Item Box

Gets the time length of the next recording.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property RecordLengthTime As Double
C# 
public abstract double RecordLengthTime {get;}
C++/CLI 
public:
abstract property double RecordLengthTime {
   double get();
}

Remarks

Use RecordLength or SetRecordLength to set the recording length.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also