Keysight 89600 VSA .NET API
SegmentedCaptureDuration Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Recording Class : SegmentedCaptureDuration Property


Glossary Item Box

Gets or sets the recording-specific segmented-capture duration (or timeout), in seconds.

Syntax

Visual Basic (Declaration) 
Public Overridable Property SegmentedCaptureDuration As Double
C# 
public virtual double SegmentedCaptureDuration {get; set;}
C++/CLI 
public:
virtual property double SegmentedCaptureDuration {
   double get();
   void set (    double value);
}

Remarks

This value applies only to variable-length segmented capture (Time.SegmentType is SegmentType.VariableLength) when the Time.SegmentedCaptureLengthType is SegmentedCaptureLengthType.CountAndTimeout (where it is the recording's timeout) or SegmentedCaptureLengthType.CountAndDuration (where it is the recording's observation duration). It is independent of the measurement's Time.SegmentedCaptureDuration because a recording may capture a different amount of data than the live measurement.

When SegmentedCaptureDurationAuto is True this value is computed automatically and this property will reflect what was automatically computed.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also