| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property SegmentedCaptureDurationAuto As Boolean | |
| C# | |
|---|---|
public virtual bool SegmentedCaptureDurationAuto {get; set;} | |
When True (the default), the recording's segmented-capture duration/timeout is computed from the measurement's Time.SegmentedCaptureDuration scaled by the ratio of the recording's segment count to the measurement's Time.SegmentCount. When False, the value set with SegmentedCaptureDuration is used. When SegmentedCaptureDuration is set, this property is set to false; setting this property back to true discards that value and computes SegmentedCaptureDuration automatically again.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00