| Visual Basic (Declaration) | |
|---|---|
Public Event PropertyChanged As PropertyChangedEventHandler | |
| C# | |
|---|---|
public event PropertyChangedEventHandler PropertyChanged | |
| C++/CLI | |
|---|---|
public: event PropertyChangedEventHandler^ PropertyChanged | |
The event handler receives an argument of type PropertyChangedEventArgs containing data related to this event. The following PropertyChangedEventArgs properties provide information specific to this event.
| Property | Description |
|---|---|
| PropertyName |
The PropertyChanged event cannot be used directly when crossing an System.AppDomain boundary, which occurs when accessing the Keysight 89600 VSA software application programming interface (API) from a macro or external client application. See NotifyPropertyChangedWrapper for information on how to receive PropertyChanged notifications.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)