| Visual Basic (Declaration) | |
|---|---|
Public Event PropertyInfoChanged As EventHandler(Of PropertyInfoChangedEventArgs) | |
| C# | |
|---|---|
public event EventHandler<PropertyInfoChangedEventArgs> PropertyInfoChanged | |
| C++/CLI | |
|---|---|
public: event EventHandler<PropertyInfoChangedEventArgs^>^ PropertyInfoChanged | |
The event handler receives an argument of type PropertyInfoChangedEventArgs containing data related to this event. The following PropertyInfoChangedEventArgs properties provide information specific to this event.
| Property | Description |
|---|---|
| PropertyName | Gets the name of the property whose information has changed. |
The PropertyInfoChanged event cannot be used directly when crossing an System.AppDomain boundary, which occurs when accessing the Keysight 89600 VSA software application programming interface (API) from a macro or external client application. See NotifyPropertyInfoChangedWrapper for information on how to receive PropertyInfoChanged notifications.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)