| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsResolutionBandwidthAuto As Boolean | |
| C# | |
|---|---|
public abstract bool IsResolutionBandwidthAuto {get; set;} | |
When true, the RBW is chosen based upon the SpanToResolutionBandwidthRatio and IsSpanToResolutionBandwidthRatioAuto settings. When false the RBW is explicitly specified via the ResolutionBandwidth property. This property defaults to true.
This property is ignored when in zero span mode.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)