Keysight 89600 VSA .NET API
PositiveMask Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Status Class : PositiveMask Property


Glossary Item Box

Gets or sets the status bits to include in PositiveValue when bit is set.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PositiveMask As StatusBits
C# 
public abstract StatusBits PositiveMask {get; set;}
C++/CLI 
public:
abstract property StatusBits PositiveMask {
   StatusBits get();
   void set (    StatusBits value);
}

Property Value

a bitwise-OR of StatusBits enumeration values

Remarks

Whenever a bit in the PositiveMask property transitions from unset to set, the bit is added to the PositiveSummary property.

You can watch for this transition by polling the PositiveSummary property, or you can register for a property change event on the PositiveSummary property (subscribing to a property change event handler for the Measurement.Status object and watching for PositiveValue to change).

For an example, see the description of the Status class itself.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also