| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property PositiveSummary As StatusBits | |
| C# | |
|---|---|
public abstract StatusBits PositiveSummary {get;} | |
| C++/CLI | |
|---|---|
public: abstract property StatusBits PositiveSummary { StatusBits get(); } | |
Reading the PositiveSummary property returns a value that corresponds to the summation of all the status bits in the PositiveMask property that transitioned from negative to positive since PositiveSummary was last read.
Reading the PositiveSummary property clears it as well so make sure you read it into a local variable if you want to test for multiple status bits.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)