Keysight 89600 VSA .NET API
Time Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Time Class


Glossary Item Box

The Time object contains members for controlling time-related measurement features.

Object Model

Time ClassTimeChannelCollection ClassTimeChannel Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Time 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Remarks

The Time object represents the frequency settings of the measurement, including time length, gating, overlap, etc.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also