Keysight 89600 VSA .NET API
Time Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Time Class

Glossary Item Box

The following tables list the members exposed by Time.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyChannelsGets the collection of TimeChannel objects representing the per-channel time settings.  —
Public PropertyGateDelayGets or sets the time gate delay for all channels, in seconds.  —
Public PropertyGateLengthGets or sets the time gate length, in seconds.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsGateGets or sets a value indicating whether time gating is enabled.  —
Public PropertyIsResolutionAutoGets or sets a value indicating whether the span is adjusted to achieve specified main time length.  —
Public PropertyIsSegmentedCaptureGets or sets a value indicating whether the measurement should use segmented capture.  19.00
Public PropertyLengthGets or sets the main time length, in seconds.  —
Public PropertyOverlapGets or sets the maximum amount of overlap processing when averaging is off, in percent.  —
Public PropertyOverlapAverageGets or sets the maximum amount of overlap processing when averaging is on, in percent.  —
Public PropertyPointsGets or sets the number of main time points.  —
Public PropertySegmentCountGets or sets the number of segments to acquire when doing segmented capture.  19.00
Public PropertySegmentedCaptureDurationGets or sets the total desired segmented capture duration in seconds.  25.40
Public PropertySegmentedCaptureLengthTypeGets or sets how the overall segmented capture length is specified  25.40
Public PropertySegmentTypeGets or sets what kind of segment length to use  25.40
Public PropertySelectedSegmentGets or sets the selected segment to analyze.  19.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also