| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property SegmentCount As Integer | |
| C# | |
|---|---|
public virtual int SegmentCount {get; set;} | |
Property Value
The minimum value is 1. The maximum is determined by the limits of the input hardware (or recording). The default value is 10 unless the input hardware or recording limits it to less than that.This value is ignored unless IsSegmentedCapture is true.
When SegmentType is set to SegmentType.VariableLength then this property specifies the desired segment count, but the capture will finish before this value if the hardware acquisition memory fills up before the count specified.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 19.00