| Overload | Description |
|---|---|
| Create() | Create a new trace and add it to the end of the Trace collection. |
| Create(Int32) | Create new traces and add them to the end of the Trace collection. |
| Create(String[]) | Create new traces and add them to the end of the Trace collection. |
| Create(String) | Create a new trace and add it to the end of the Trace collection. |
| Create(String,Boolean,Boolean) | Create a new Trace or return a existing Trace. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)