Keysight 89600 VSA .NET API
Create(String) Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TraceCollection Class > Create Method : Create(String) Method


dataName
The initial contents (Trace.DataName) of the new trace.

Glossary Item Box

Create a new trace and add it to the end of the Trace collection.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function Create( _
   ByVal dataName As String _
) As Trace
C# 
public abstract Trace Create( 
   string dataName
)
C++/CLI 
public:
abstract Trace^ Create( 
   String^ dataName
) 

Parameters

dataName
The initial contents (Trace.DataName) of the new trace.

Return Value

The new Trace.

Remarks

The new trace is not initially Visible (Trace.IsVisible).

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also