Keysight 89600 VSA .NET API
DataNamesMeasurement Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TraceCollection Class : DataNamesMeasurement Method


measurementIndex
The index of the measurement.

Glossary Item Box

Gets the list of all measurement DataNames for the specified measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function DataNamesMeasurement( _
   ByVal measurementIndex As Integer _
) As String()
C# 
public abstract string[] DataNamesMeasurement( 
   int measurementIndex
)
C++/CLI 
public:
abstract array<String^>^ DataNamesMeasurement( 
   int measurementIndex
) 

Parameters

measurementIndex
The index of the measurement.

Return Value

An array of all the measurement data names.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also