Keysight 89600 VSA .NET API
DefaultDataNamesMeasurement Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TraceCollection Class : DefaultDataNamesMeasurement Method


measurementIndex
The index of the measurement.

Glossary Item Box

Gets the list of all default measurement DataNames for the specified measurement.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function DefaultDataNamesMeasurement( _
   ByVal measurementIndex As Integer _
) As String()
C# 
public abstract string[] DefaultDataNamesMeasurement( 
   int measurementIndex
)
C++/CLI 
public:
abstract array<String^>^ DefaultDataNamesMeasurement( 
   int measurementIndex
) 

Parameters

measurementIndex
The index of the measurement.

Return Value

The default data names for the measurement.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also