Keysight 89600 VSA .NET API
ValidGraphDataNames Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > TraceCollection Class : ValidGraphDataNames Property


Glossary Item Box

Gets the list of all DataNames that are valid to use as input to a Graph.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property ValidGraphDataNames As String()
C# 
public virtual string[] ValidGraphDataNames {get;}
C++/CLI 
public:
virtual property array<String^>^ ValidGraphDataNames {
   array<String^>^ get();
}

Property Value

The valid data names for a Graph.

Remarks

These DataNames can be used for the StimulusDataName and ResponseDataName properties.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 17.00

See Also