Applies filtering when rendering the trace data, based on the filter type and values provided.
Syntax
Parameters
- filterType
- Specifies the type of filtering to apply.
- filterValues
- Specifies the values to filter out of the drawing. Any values not found in the filterValues will remain enabled in the drawing.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 23.20
See Also