Keysight 89600 VSA .NET API
UserInputChangeBits Enumeration
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserInputChangeBits Enumeration


Glossary Item Box

Flags indicate property changes related to UserInputData properties.

Syntax

Visual Basic (Declaration) 
Public Enum UserInputChangeBits 
   Inherits System.Enum
C# 
public enum UserInputChangeBits : System.Enum 
C++/CLI 
public enum class UserInputChangeBits : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
IsContinuousIndicates change occurred to UserInputData.IsContinuous.—
IsRequiredSamplesPositiveIndicates change occurred to make UserInputData.RequiredSamples positive (which indicates data s requested by the data consuming Measurement).—
IsTriggeredIndicates change occurred to UserInputData.IsTriggered.—
NoneIndicates no changes (Default value).—
RequestedBlockSizeIndicates change occurred to UserInputData.RequestedBlockSize.—
RequestedTriggerDelayIndicates change occurred to UserInputData.RequestedTriggerDelay.—
SettlingSizeIndicates change occurred to UserInputData.SettlingSamples.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also