| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property RequiredSamples As Long | |
| C# | |
|---|---|
public abstract long RequiredSamples {get;} | |
Returns the number of floats (2x samples if UserInputSetup.IsComplexData is true) that the data consuming Measurement is waiting for to perform the next measurement update. The value of this property changes as data is input via the SendData(IEnumerable<Single[]>) method. A zero or negative return value indicates that the data consuming Measurement is not waiting for data points (if negative, a surplus is implied). With overlapped processing, this property will increment by a value that is generally less than the measurement block size after a measurement update. This property gets the property value of the first channel. Use Channels to get or set properties of individual channels. Changes to this read-only property may be detected through UserInputChangeRegister.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)