Keysight 89600 VSA .NET API
UserInputData Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserInputData Class

Glossary Item Box

The following tables list the members exposed by UserInputData.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAcquisitionStatusGets or sets the acquisition status feedback from the data source application.  —
Public PropertyChannelsGets the interface for channelized (on a per input channel basis) properties and methods for processing data transfers from a data source application.  —
Public PropertyIsContinuousGets a value indicating whether the data consuming Measurement is operating in continuous (overlapped) mode.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsMeasurementEnabledGets or sets a value indicating whether the attached measurement is enabled.  —
Public PropertyIsOverloadedGets or sets a value indicating whether a range overload has occurred.  —
Public PropertyIsTriggeredGets a value indicating whether the data consuming Measurement is operating in triggered mode.  —
Public PropertyRequestedBlockSizeGets the amount of data requested to complete a single measurement update.  —
Public PropertyRequestedTriggerDelayGets the requested trigger delay, in seconds, relative to the first data sample.  —
Public PropertyRequiredSamplesGets the amount of data required to update the current measurement.  —
Public PropertySettlingSamplesGets the amount of data expected to be needed for settling.  —
Public PropertyTriggerDelayGets or sets the trigger delay, in seconds, for data to be processed by the current measurement update.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodClearDataClears unprocessed data.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSendDataOverloaded. Send data to be processed.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also