Keysight 89600 VSA .NET API
UserInputSetup Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserInputSetup Class


Glossary Item Box

Contains properties and methods to define properties of the data source application.

Object Model

UserInputSetup ClassUserInputSetupChannelCollection ClassUserInputSetupChannel Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class UserInputSetup 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class UserInputSetup abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also