Keysight 89600 VSA .NET API
UserInputSetup Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : UserInputSetup Class

Glossary Item Box

The following tables list the members exposed by UserInputSetup.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyBandwidthGets or sets the alias-protected bandwidth (maximum span) the data consuming Measurement should assume for data provided by data source application.  18.0
Public PropertyCaptureSizeMaximumGets or sets whether the input data will have gaps, this is the minimum gap-free length that will be available after each gap.  —
Public PropertyCenterFrequencyGets or sets the center frequency the data consuming Measurement should assume for data provided by data source application.  —
Public PropertyChannelsGets an interface to channelized (on a per input channel basis) properties and methods for defining properties of the data source application.  —
Public PropertyIsComplexDataGets or sets a value indicating whether complex data will be provided by data source application.  —
Public PropertyIsContinuousCapableGets or sets a value indicating whether continuous acquisitions are supported by data source application.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsImmediateChangesEnabledGets or sets a value indicating whether property changes should be processed immediately. If false, ApplyChanges should be called by the data source application to initiate processing of property changes. Default value is false. If true, property changes will be processed immediately. Processing changes has the affect of causing the data consuming Measurement to be preset to a default state. It will also cause any data in the internal buffers to be cleared.  15.00
Public PropertyIsTriggeredCapableGets or sets a value indicating whether data source application supports triggered data acquisitions.  —
Public PropertyRangeGets or sets the input range to associate with data from the data source application.  —
Public PropertySampleRateGets or sets the sample rate the data consuming Measurement should assume for data provided by data source application  —
Public PropertyTriggerDelayMaximumGets or sets the maximum trigger delay, in seconds, the data source application is capable of configuring.  —
Public PropertyTriggerDelayMinimumGets or sets the minimum trigger delay, in seconds, the data source application is capable of configuring.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodApplyChangesProcessed any pending changes.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodSetFrequencyParametersOverloaded. Sets frequency parameters.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also