Keysight 89600 VSA .NET API
Create() Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > ContextCollection Class > Create Method : Create() Method


Glossary Item Box

Create a new, empty Context using the default ContextExtension type, and default Context.Name.

Syntax

Visual Basic (Declaration) 
Public Overloads MustOverride Function Create() As Context
C# 
public abstract Context Create()
C++/CLI 
public:
abstract Context^ Create(); 

Return Value

A handle to the newly created context.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also