| Visual Basic (Declaration) | |
|---|---|
Public Overloads MustOverride Function Create( _ ByVal contextExtensionType As Type _ ) As Context | |
| C# | |
|---|---|
public abstract Context Create( Type contextExtensionType ) | |
| C++/CLI | |
|---|---|
public: abstract Context^ Create( Type^ contextExtensionType ) | |
Parameters
- contextExtensionType
- Type to use for ContextExtension of new Context.
Return Value
A handle to the newly created context.| Exception | Description |
|---|---|
| System.ArgumentException | Thrown if contextExtensionType is not supported. |
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)