| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function RemoveAt( _ ByVal index As Integer _ ) As Boolean | |
Parameters
- index
- Zero-based index of Context to remove from the collection
Return Value
True, if the Context was removed from the collection.Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)