Keysight 89600 VSA .NET API
RemoveAt Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > EventActionCollection Class : RemoveAt Method


index
index of EventAction to remove

Glossary Item Box

Remove the EventAction at the specified index.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function RemoveAt( _
   ByVal index As Integer _
) As Boolean
C# 
public abstract bool RemoveAt( 
   int index
)
C++/CLI 
public:
abstract bool RemoveAt( 
   int index
) 

Parameters

index
index of EventAction to remove

Return Value

true if successful, false otherwise

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also