Keysight 89600 VSA .NET API
EventAction Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : EventAction Class


Glossary Item Box

An EventAction performs a particular action based on a EventRule.

Syntax

Remarks

The type of action to be performed is defined by Keysight.SA.Vsa.EventAction.SetExtension``1. The settings can be used to configure the EventAction.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also