Keysight 89600 VSA .NET API
SetExtension Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > EventAction Class : SetExtension Method


Glossary Item Box

Changes the current EventActionExtension to the indicated type (if necessary) and returns an appropriately typed handle to the EventActionExtension object.

Overload List

OverloadDescription
SetExtension<T>()Changes the current EventActionExtension to the indicated type (if necessary) and returns an appropriately typed handle to the EventActionExtension object.  
SetExtension(Type)Changes the current EventActionExtension to the indicated type (if necessary) and returns a handle to the EventActionExtension object.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also