T
The type to which to cast the returned EventDataSourceExtension.
Keysight 89600 VSA .NET API
GetExtension<T> Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > EventDataSource Class : GetExtension<T> Method


Glossary Item Box

Returns the current EventDataSourceExtension cast to the requested type.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetExtension(Of T As EventDataSourceExtension)() As T
C# 
public abstract T GetExtension<T>()
where T: EventDataSourceExtension
C++/CLI 
public:
abstract T^ GetExtensiongeneric<typename T>
(); 
where T: EventDataSourceExtension

Type Parameters

T
The type to which to cast the returned EventDataSourceExtension.

Return Value

The current EventDataSourceExtension cast to the requested type, or null if the current EventDataSourceExtension is not of the requested type.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also