Keysight 89600 VSA .NET API
EventDataSource Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : EventDataSource Class


Glossary Item Box

An EventDataSource supplies data for the EventCondition of an EventRule.

Syntax

Remarks

The type of data source is defined by Keysight.SA.Vsa.EventDataSource.SetExtension``1. The extension object can be used to configure the EventDataSource.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also