Keysight 89600 VSA .NET API
GetAvailableExtensionTypes Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace > EventRule Class : GetAvailableExtensionTypes Method


Glossary Item Box

Gets the list of available EventCondition types that can be used. Use the Keysight.SA.Vsa.EventRule.SetExtension``1 method to select which EventCondition is used.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetAvailableExtensionTypes() As Type()
C# 
public abstract Type[] GetAvailableExtensionTypes()
C++/CLI 
public:
abstract array<Type^>^ GetAvailableExtensionTypes(); 

Return Value

array of EventCondition types

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also