Keysight 89600 VSA .NET API
EventRule Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Keysight.SA.Vsa Namespace : EventRule Class


Glossary Item Box

A EventRule defines which Actions to perform, based on a particular EventCondition, based on the data from the DataSources

Object Model

EventRule ClassEventActionCollection ClassEventAction ClassEventAction ClassEventAction ClassEventCondition ClassEventDataSourceCollection ClassEventDataSource ClassEventDataSource ClassEventDataSource Class

Syntax

Remarks

The rule's condition is defined by Keysight.SA.Vsa.EventRule.SetExtension``1. The condition object can be used to configure the EventCondition.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also